Cancel
Showing results for 
Search instead for 
Did you mean: 

Shaft Threading

Creator
Creator

I'm trying to create a thread along a shaft (1-8 thread on a 1"x 6" shaft - nothing unusual) and I keep receiving this error:

Error.JPG

I can make threads up to 3", but anything longer and I receive the same error. I've tried threading on a few different shafts (including a couple metric) on different models and receive the same error. Anyone have any ideas? I've restarted the program, opened different models, tried offset starting planes, pitches, diameters, etc. with no luck.

12 REPLIES 12

Re: Shaft Threading

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Is your thread a swept feature? This message can occur when faces/edges on tool bodies touch faces/edges on target bodies, for example, if the inner face of a swept thread tool body has the same diameter as the outer face of the shaft it is to be united to. In these cases the message can be prevented by making the the two bodies physically interfere rather than touch.

Regards, Ben

Re: Shaft Threading

Creator
Creator

If I use 3" as the thread length I get this:

thread2.JPG

If I set it at 3.1" I get the error message:

Error.JPG

 

 

Re: Shaft Threading

Creator
Creator

This is using the Thread tool set on Detailed.

Re: Shaft Threading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you using the "thread" command or are you creating the thread manually?

 

If you are creating the thread manually, take a look here. There is a file attached that illustrates what @BenBroad mentioned.

 

Edit (didn't see the latest replies): since you are using the thread tool, you should report this behavior to GTAC so they can investigate (and hopefully fix) it.

Re: Shaft Threading

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Looks like a similar PR was reported: PR 7878783. It's still open, and on it's way to Parasolid Development to review. You can open an IR with GTAC to have you notified when the problem has been fixed.

Regards, Ben

Re: Shaft Threading

Creator
Creator

Thread Command. I'm used to cutting the threads manually in Solidworks, I just thought this was a novel tool in NX, but I haven't had a ton of success with it.

Re: Shaft Threading

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
It's an old command. Probably due to be revamped Smiley Happy

Re: Shaft Threading

Honored Contributor
Honored Contributor

In much need of a revamp, works better with the hole callout, to dimension them.

 

 

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Shaft Threading

Phenom
Phenom

Unless you manufacture the threads, it’s not a best practice in Solidworks to make physical thread Cut Sweeps and it’s highly discouraged. Instead it offers to use Standard Cosmetic Thread symbols, face colouring and simplified screws (liner cut pattern type). Basically, why do you want to waste system resources unnecessarily on the purchased Standard components?

I’m not sure about NX best practices in this regards. But I’ve seen some NX users prefer and don’t mind to load the Reuse Library/ Part family with all the internal detail with smart features. Any NX veterans like to share your thoughts or best practices?  

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW