Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal flanges overlapping ? No gaps.

Genius
Genius

Hi

NX doesn't automatically adjust gaps when bending flanges...

  • So I end up with a lots of closed overlapping FLAT-PATTERN bends. Now I manually make gaps to them.
  • How much space should I leave on gaps(=gap width) on each sheetmetal ?
  • Is it like 1mm thick=1mm gap and 2mm thick=2mm gap when bending ?

Gap width.jpg

2 REPLIES

Re: Sheet metal flanges overlapping ? No gaps.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @12131444,

 

I don't believe the answer is just so straight forward. The bending is different for each machine. And also corresponding to the Tools used in the machine. Not sure about how it's call. But I believe it has to do with "knife" used. Sharp/blunt. And the side where it's pressed into.

 

Maybe others can give you practical tips/tricks of the real life Smiley Happy

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Sheet metal flanges overlapping ? No gaps.

Gears Legend Gears Legend
Gears Legend

Hi,

 

If you want to be very exact with this desired dimension you will have to;

 

-Use exact bend data (Bend Radius and Neutral Factor ) As Dennis already mentioned this will be depending on:

  • material type used
  • material thickness
  • bend angle
  • nose radius of the bend punch
  • V-die width

-Unbend the specific bend and manually add material with e.g. a Secondary Tab. Then rebend. That way you will be 100% sure that the gap will be what you want it to be in the flat pattern.

 

BTW: In your drawing the horizontal gap is driven by the Bend Relief Width.

When working with the actual bend radii (that reflect reality) the bend relief DEPTH can always be set to zero (0); The bend relief depth is there to prevent that an inset bend radius will tear his way into the adjacent tab. This "tearing" will be more visible with thicker and stronger materials.

 

I hope this helps.

 

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend