Cancel
Showing results for 
Search instead for 
Did you mean: 

Siemens NX 11 tool/machinery library

Experimenter
Experimenter

For my internship project I install a update for Siemens NX 11, after the update I have lost my tool library. My internship supervisor is abroad for a project, so it is not possible to ask the webkey codes. Is ther a outher way I can download a new machinery tool library?

 

I need to have a solution fast?

 

 

Capture.PNG

 

 

3 REPLIES 3

Re: Siemens NX 11 tool/machinery library

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
In my opinion, an update should not result in loosing your parts in the Reuse Library ?! Perhaps only the paths are wrong. You can find the desired paths in the Customer Default > Reuse Library > General > Native NX

Re: Siemens NX 11 tool/machinery library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And the required codes to crceate a webkey account are available in NX by using File -> Help -> Log file

Then scrolling down a little bit

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Siemens NX 11 tool/machinery library

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

What was the previeus version of NX that they are using there?

Was the update that you did of a NX version up or installing a new MR?

 

If its a version up can you then open the old NX version?

If so go to the reuse library navigator->right click on the Grey Name row->Library Management.

Here you can check where the libraries are located.

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions