Cancel
Showing results for 
Search instead for 
Did you mean: 

Simplify body command

Creator
Creator

Dear All

I would like to use "Simplify body". I search in command finder as picture.

I set the environment as recommend. But this cammand can't use or add to any toolbar.

Do you have any suggestion?

Thank you.

NX10.0.3 Mp03

windows7 64bit

 

3 REPLIES

Re: Simplify body command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use the synchronous commands instead (delete face, move face, replace face, etc).

Re: Simplify body command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In addition if you set this variable new capabilities of the cap face are removed from the synchronous modeling delete face dialog.

Delete face of synchronous modeling has got much better over the last few releases, so you should really not need simplify body any more.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Simplify body command

Creator
Creator

Dear All

Thank you for your reccommend .

But some colleague need to use old command.