Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketch Constraint Color

Pioneer
Pioneer

Hello,

 

One of the student raised the question why NX ( be it NX9 or NX11) does not show sketch constraint status color after finishing the constraint.
See attached sketch colours from the preferences.

 

We are able to see the particular color for ex. partially constrained as brown; but the moment we finish the constraint dialogue (geometric/dimensional) we don't have the required display.

 

Can any one raise a PR for this? Thanks.

Durgavajjala S.Prasad /NX 9,NX10&NX11
7 REPLIES 7

Re: Sketch Constraint Color

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @NXplorer,

 

A similar PR was reported: PR 6384700 and closed as Enhancement (EN).

The only colors you will see outside of constraining (dimensional and geometric) are for conflicting and over-defined cases.

 

Regards, Ben

Re: Sketch Constraint Color

Siemens Phenom Siemens Phenom
Siemens Phenom

Also refer the following post and comment from @BenBroad

NX 11 fully constraint sketch color not showing ??

 

"When Continuous Auto Dimensioning is enabled, the sketch ends up as fully constrained. In this mode, it isn't helpful to change all the curves to a new color. The color coding for constraint status is only useful when some geometry is underconstrained. If the user disables Continuous Auto Dimensioning, then it is possible to get underconstrained geometry and the color coding is used."

Re: Sketch Constraint Color

Pioneer
Pioneer

Just wonder PR as old as 2010 still a distant dream? Eager to see realization of EN.

Durgavajjala S.Prasad /NX 9,NX10&NX11

Re: Sketch Constraint Color

Legend
Legend

Hi

Do you meaned 'you can see each color only while Contrain or Dimension Dialogue are actived'?
If I understood you well, it is just regular.

 Sunkap Ahn, Senior Support Engineer


logo

Re: Sketch Constraint Color

Pioneer
Pioneer
Agreed!
Durgavajjala S.Prasad /NX 9,NX10&NX11

Re: Sketch Constraint Color

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @NXplorer,

 

Just wonder PR as old as 2010 still a distant dream? Eager to see realization of EN.

By mentioning the existing PR# I had hoped to prevent unnecessary time & effort for you and GTAC Smiley Happy and that you could simply request that you be added to the existing ER.

Since the functionality (with respect to the sketch colors) hasn't changed since NX7.5 (when the PR was submitted), one should assume that the ER is still valid - though I can't comment on the realization.

 

Regards, Ben

Re: Sketch Constraint Color

Pioneer
Pioneer
Thanks Ben!
Durgavajjala S.Prasad /NX 9,NX10&NX11