Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketch's dimension creates only horizontal measures ?

Genius
Genius

Hello

Sketch's dimension creates only horizontal measures.

  • NX wants to create just the orange horizontal dimension ( Circled with red ).
  • Why it does not want to create the needed vertical dimension ( Drawed black line )
  • It happens only in this model.
  1. Replace Reference Set = "entire part".

 

5656565.jpg

3 REPLIES 3

Re: Sketch's dimension creates only horizontal measures ?

Genius
Genius

Ok. Measurement Method was set in Inferred instead of Vertical.

Now it works.

adadaff.jpg

 

Highlighted

Re: Sketch's dimension creates only horizontal measures ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi, 

Are the two points exactly vertically aligned or there is some deviation(sorry i could not validate it using the picture only but may be there is a very small deviation).

Best Regards

Kapil

Re: Sketch's dimension creates only horizontal measures ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Smiley Happy i was too slow with my post...please ignore as you already got the solution.