Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketching in draftings wont snap to geometry

Experimenter
Experimenter

Hi, I want to make skatches in drafting, but if I make some sketches the will not snap to any geometry. I can make it in other programs, but not in NX10. Can someone tell me how to do it?

4 REPLIES 4

Re: Sketching in draftings wont snap to geometry

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you using the master Master Model approach?

 

Is this an assembly drawing?

 

Do you receive any messages or information indicating something is wrong?

Re: Sketching in draftings wont snap to geometry

Pioneer
Pioneer

Would you give some more details on it ?

 

If possible attach some screenshots

 

/Sathyaraj

Re: Sketching in draftings wont snap to geometry

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

typical issue here is that the sketch can only snap to geometry in the active sketch view. So if you create a sketch on the drawing it cannot reference geometry created in a view.

So make sure you select the view and use right mouse button -> Active Sketch view. Then draw the sketch in the view.

 

Hope that helps,

Johannes

 

Re: Sketching in draftings wont snap to geometry

Pioneer
Pioneer

Adding to johannes point, turn on the later setting pertaining to that view, as well as layer settings for the drawing.