Cancel
Showing results for 
Search instead for 
Did you mean: 

Snapshot view

Creator
Creator

Hi,

Since which version of NX is it possible to add a snapshot view on a draft part?

 

 

6 REPLIES 6

Re: Snapshot view

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Luvi,

There is an enhancement introduced in NX 11.0.1 as "Locking views" which includes 'Snapshot' as one of the view locking methods.

Re: Snapshot view

Creator
Creator

Hi,

I know that the snapshot view option already avalaible was in NX9, but before NX9 was is already avalaible?

 

Re: Snapshot view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Snapshot" is an option in NX 8.5 (the oldest version of NX that I currently have installed to check). I don't remember when it first appeared, but IIRC, it was an option in versions earlier than NX 8.5.

Re: Snapshot view

Creator
Creator

Thankyou

Re: Snapshot view

Siemens Phenom Siemens Phenom
Siemens Phenom

@Luvi, I misunderstood your question completely.

Are you referring to command 'Create Snapshot Data' of 'Track Drawing Changes' functionality?

Re: Snapshot view

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@Luvi,

 

@cowski1 is correct.  NX8.5 was the earliest. 

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration