Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid to surfaces for CFD

Gears Phenom Gears Phenom
Gears Phenom

NX 9.0.3

 

Our aero department has asked if we(design department) can come up with a method within NX to convert our solid bodies in to water tight sheet bodies.

 

Ideally the workflow would be fairly simple, so the aero guys can do it, without extensive NX training, with traceability back to the original "master model".

 

Has anyone done anything like this in NX?

 

One of the aero guys mentioned they used ANSA as an intermediate software, between CAD and Star ccm+ (CFD software).  We want to avoid a third piece of software, staying in NX until it's ready to go to CFD.

 

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
4 REPLIES

Re: Solid to surfaces for CFD

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried using the 'Unsew' function?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Solid to surfaces for CFD

Gears Phenom Gears Phenom
Gears Phenom

That sounds very promising, thanks.

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Solid to surfaces for CFD

Siemens Legend Siemens Legend
Siemens Legend
how does the process look ?
you have the NX solid, then .... and after that Star CCM?

I imagine that if you open the NX file in ANSA and ANSA only can use sheet bodies, the NX solid will suddenly have become a sheet body?
Or is it ANSA that you want to avoid ?


Regards,
Tomas

Re: Solid to surfaces for CFD

Gears Phenom Gears Phenom
Gears Phenom

We are trying to avoid ANSA.

 

I showed the CFD guys, and they are testing the process to see what they think.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1