Cancel
Showing results for 
Search instead for 
Did you mean: 

Split Mold

Pioneer
Pioneer

Hello,

I have question ?

How to create split mold in NX by using moldwizard ?

I know manually but not automatically.

When i try to create parting surface in mold wizard it is in horizontal position but i want it to be in vertical position?

2 REPLIES

Re: Split Mold

Valued Contributor
Valued Contributor

Without seeing it, I would say that you need to change the vector of the parting segment in the "Design Parting Surface" dialog. Adding guidelines may help it work "automatically".

Re: Split Mold

Pioneer
Pioneer

This is the component which i used.