Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Spreadsheet. "Failed to set Excel running"

Valued Contributor
Valued Contributor

Dear Users and Experts,

 

I place a new spreadsheet in a drawing of mine and then want to edit it with Excel.

But I get the message only: "Failed to set Excel running".

Does anybody have an idea what is wrong here?

 

NX Version 12.0.2.9

Microsoft Office 2010

Windows 10

 

How to connect NX with Excel?

 

 

Many thanks for your advices

 

 

22 REPLIES 22

Re: Spreadsheet. "Failed to set Excel running"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Blendy ,

 

Does your spreadsheet contains complex formulas or validation or it's just blank file?

 

Try performing Part Cleanup and see if it helps.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Spreadsheet. "Failed to set Excel running"

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Do you have an Excel session running in the background when you try to use the Drafting Spreadsheet?  If you don't open up Task Manager and see if there are any Excel processes running.  If there are, kill them and then attempt to access the Drafting Spreadsheet.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Spreadsheet. "Failed to set Excel running"

Valued Contributor
Valued Contributor

Thank you for your answers.

 

Maybe I have to add that we just have installed NX 12 a short time ago. On a brand new PC. Maybe we even haven't installed NX12 and Excel correctly.

Our Offices 2010 (including Excel) works, though.

Maybe one has to set some paths or something in NX 12 to enable NX 12 to find the connection to Excel?

 

I also remember from earier versions (before NX6 ) that is was important in which chronological order NX12 and Excel is installed on the PC. But I forgot what order was correctly. And maybe it works differently these days.

 

Re: Spreadsheet. "Failed to set Excel running"

Valued Contributor
Valued Contributor
we just put a new table on the drawing with a few rows and columns. Then we use the "Edit using Spreadsheed" command. But we only get the message "Failed to set Excel running".

Re: Spreadsheet. "Failed to set Excel running"

Valued Contributor
Valued Contributor
there are no Excel processes in the background, neither before the "Edit using Spreadsheet" command nor after that.

Re: Spreadsheet. "Failed to set Excel running"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Blendy,

With reference to NX compatibility with Spreadsheet, MS Excel 2010 (32–bit) is supported for NX12 on Windows 10 platform.

 

Do you have any old version of office/excel installed on same system?

 

Re: Spreadsheet. "Failed to set Excel running"

Valued Contributor
Valued Contributor
Computer is brand new, Office 2010 and NX12 installed. No older Office versions. Smiley Happy

Re: Spreadsheet. "Failed to set Excel running"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Blendy,

 

As @GaneshKadole has mentioned... Office 32-bit is supported, 64-bit is not!

As you sure you have the 32-bit version installed?

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Spreadsheet. "Failed to set Excel running"

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Blendy 

 

Please create a new part file, using the Blank template on the File > New dialog, and repeat your steps.  Let us know the result.  Do you get the same error if you select "Tools > Spreadsheet" and if you repeat the steps in the Modeling Application?

 

Thanks, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration