Cancel
Showing results for 
Search instead for 
Did you mean: 

Start the light tracking static image rendering, the computer stuck CPU occupied 100%

Pioneer
Pioneer

hello all

Start the light tracking static image rendering sdsd.png  ,The computer will become very card graphics window can not rotate. the computer stuck CPU occupied 100% What is the reason? My graphics card is NVIDIA GTX750Ti.Given the material when the material is also very Dayton,

When rendering can be used without using the CPU only use the GPU, because I found that sometimes use the CPU to cause the computer to crash.

2.I do not want the light trace to open and cause the computer Caton model to not rotate.
keyshot rendering will not cause the computer card, NX start ray tracking window after feeling nx fluency will be worse, the software becomes very card, can not smooth operation nx.

 

 

无标题.png

3 REPLIES

Re: Start the light tracking static image rendering, the computer stuck CPU occupied 100%

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @FZK,

 

The graphics adapter you refer to (NVIDIA GTX750Ti) is what nVidia refers to as a "gaming" device.  While it it meets the requirements for CUDA Compute Capability 2.0 and higher (make sure your driver supports CUDA 8.0 or higher), it's suitable to render objects using keyshot, and you're able to use NX, the device is not intended to be used for high-end accelerated open GL applications, such as NX.

The nVidia website has a page dedicated to devices that have been benchmarked, recommended and certified, for Siemens products.  The Siemens GTAC website also has a list of hardware, including graphics adapters, that have been certified for SPLM products.

 

Regards, Ben

Re: Start the light tracking static image rendering, the computer stuck CPU occupied 100%

Pioneer
Pioneer

hello BenBroad

Thank you, I downloaded from the NVIDIA website WIN10 latest driver to solve the current problem,
thank you very much

 

Re: Start the light tracking static image rendering, the computer stuck CPU occupied 100%

Pioneer
Pioneer

Hi SIEMENS PHENOM

How to shut down the CPU or only 60% of the CPU rendering, using only GPU rendering, static drawing rendering when NX and other applications will change the cardton.