Cancel
Showing results for 
Search instead for 
Did you mean: 

Starting .prt file through ugraf.exe

Experimenter
Experimenter

Hello everybody. On the computer there are files with the .ppt, and they are not associated with nx8.5. To do so, pushed open the file using, and then chose ugraf.exe files prt steel icon displayed with nx (seen in the screenshot) click on the file opens nx 85, but the file is still open, only through the command to open. How to make the correct association with nx85?

3 REPLIES

Re: Starting .prt file through ugraf.exe

Phenom
Phenom

Guys, he means .prt not  PowerPoint .ppt.

Re: Starting .prt file through ugraf.exe

Experimenter
Experimenter

I'm sorry, I made a typo. Yeah yeah me open prt

Re: Starting .prt file through ugraf.exe

Siemens Phenom Siemens Phenom
Siemens Phenom

hi,

Are you using Pro-E also? The file extension are same i guess (.prt) so sometimes this confusion occurs.

You can right click your file icon/Go to PROPERTIES . In GENERAL tab you need to select the ugraf.exe in OPEN WITH option.

Once this setting is done it should open in NX with a double click.

Best Regards

Kapil