Cancel
Showing results for 
Search instead for 
Did you mean: 

Stok Size command in Mold wizard application

Valued Contributor
Valued Contributor

Hey friends ,

 

I have some problem about stok size. 

For example i used stok size  for a body , next time when i open again this command ,

it's select same body automatically . 

NX 10.0.2 MP2 

It didnt work like this before NX 10 . 

Anyone know somethings about this ?

Thx for responses.

3 REPLIES

Re: Stok Size command in Mold wizard application

Phenom
Phenom

Don't you think it's better to have the body selected?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Stok Size command in Mold wizard application

Valued Contributor
Valued Contributor

i think so . Because , sometimes we can use this command without mold wizard . 

For example when we are working with different bodies in same part, i have to cancel selected and than i need to select other bodies. 

Re: Stok Size command in Mold wizard application

Experimenter
Experimenter

I agree. This command should have an option so you can run it with a one body part or a multi-body part, because once you hit apply you are stuck with that body and have the nuisance of deselecting.