Cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Spline can't select points imported from dwg file

Genius
Genius

I import a set of points from a dwg file and want to connect them to a curve. But I found that they can't be selected in Studio Spline command.

 

It seems that only points created as features are selectable in Studio Spline.

 

Can anybody give some suggestion? Thanks a lot!

2 REPLIES 2

Re: Studio Spline can't select points imported from dwg file

Siemens Phenom Siemens Phenom
Siemens Phenom

Make sure you have the Existing Point turned on in the selection bar.

 

Spline.pngPoint Selection

 

 

Scott

Re: Studio Spline can't select points imported from dwg file

Genius
Genius
It works! I had thought that imported points are different and simply forgot to check the selection rules.

Tons of thanks!