Cancel
Showing results for 
Search instead for 
Did you mean: 

Symbolic Thread - Number of Starts parameter

Legend
Legend

Hi,

 

I am trying to figure out how to speed up the creation of NX symbolic threads.

 

Everything except one thing is clear to me.

 

There is a parameter called "Number of Starts". What is the purpose of this parameter? I couldn´t figure out any change in behavior.

 

Thank you for your replies.

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5
3 REPLIES 3
Highlighted

Re: Symbolic Thread - Number of Starts parameter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

A thread with 2 starts is sometimes also called a double thread. Instead of one thread wrapping around the threaded face, there will be two. You may not see a difference in the "symbolic thread" representation.

 

https://en.wikipedia.org/wiki/Screw_thread#Lead.2C_pitch.2C_and_starts

Re: Symbolic Thread - Number of Starts parameter

Legend
Legend

Representation may not be change. However if your CAM guys are using FBM or any other method to identify the thread, program the threading operation using NX CAM, it is useful.

Re: Symbolic Thread - Number of Starts parameter

Legend
Legend
Hi Mak_Jo,

I am one of the CAM guys (but IT dept.). I'll check if any customer department has data with such a setting. Thanks!
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5