Cancel
Showing results for 
Search instead for 
Did you mean: 

TCIN - Missing dialog options icon in the title bar

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

I have TCIN setup on my machine as Teamcenter - 11.2.0 and NX 11.0.2.7 MP4.

For managed NX, dialog options icon is missing for 'Assembly Load Options' dialog, whereas for native NX it is present.

Unfortunately, I do not have TC11-NX11 setup on another machine. 

 asmloadoption.jpg

I have also checked the same for Teamenter 11, NX 10 integration, it is same. 

This may be system/setup specific issue. Need help to verify this with a similar TCIN setup.

5 REPLIES

Re: TCIN - Missing dialog options icon in the title bar

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @GaneshKadole,

 

I just tested NX9 in Tc10 and NX10/NX11 in Tc11.  The option does not exist on the dialog in Teamcenter managed NX.

 

EDIT:

I just found ER 1988290 requesting the ability to use "Save Favourite As"  on the Assembly Load Options dialog in managed mode, which would require adding "Dialog Options" to the dialog.

 

Regards, Ben

Re: TCIN - Missing dialog options icon in the title bar

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @BenBroad,

Thank you for the test and ER information.

In NX8.5 with TC9, I can see that dialog options gear icon is available for assembly load options command. Now the question is why it is not there for managed NX9/10/11? Smiley SurprisedCapture.JPG

 

Re: TCIN - Missing dialog options icon in the title bar

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Hi Ganesh,

I just confirmed that dialog options is available in NX8.5 (managed mode). Please consider opening an IR with GTAC so that they can investigate the issue for you.

Regards, Ben

Re: TCIN - Missing dialog options icon in the title bar

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Ben,

Thank you for the confirmation! I will open IR for the same.

Re: TCIN - Missing dialog options icon in the title bar

Siemens Phenom Siemens Phenom
Siemens Phenom

Solution proposal from GTAC

"As per the updates from Development it is intended design because we made the dialog Model to prevent the possibility of the user hitting outside area of the dialog. This is necessary as user can change load options from TcNav when the Assembly Load Options dialog is still up. "