Cancel
Showing results for 
Search instead for 
Did you mean: 

Tab in a note causing error

Honored Contributor
Honored Contributor

User edoted a note on a drawing (NX9), and the edit included 'tabs'.  When he tried to exit the edit, he got an error that read something like "the are required selections in the command that must be satisfied".  Take out the tabs, and replace with spaces, and it workes fine.

 

I never use tabs in notes, I suspect this was an issue in the past, could go back to the unix days?  anyway, are tabs not allowed in drawing notes?

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10
2 REPLIES 2
Highlighted

Re: Tab in a note causing error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, they aren't (or at least weren't - not sure about NX9/10)

You might want to look up the ENV variable:

UGII_DRAFT_REMOVE_UNSUPPORTED_CONTROL_CHARACTERS=TRUE

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Tab in a note causing error

Honored Contributor
Honored Contributor

I'll say tab is still not supported in NX9. 

 

ENV set, since we have a lot of (former) Solidworks users that will try.

 

Thanks Ken.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10