Cancel
Showing results for 
Search instead for 
Did you mean: 

Tabular note update affecting all sheets in draft

Experimenter
Experimenter

Hello guys,

 

I´m drafting in NX12 some operation sheets. I´m making the header of the op sheet with a tabular note that should be exactly the same on each sheet (only thing changing is sheet number). 

 

How do i set up a header that, when updated in one sheet, it gets updated on every sheet? I´m pretty sure this should be possible.

 

Thanks.

4 REPLIES 4

Re: Tabular note update affecting all sheets in draft

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @SergioG,

 

I'm assuming this is a single part file containing several sheets.   What about creating a part attribute and then referencing that attribute in your tabular note (hint: using the Relationships option in the Note editor)?

 

If you change the attribute value, each sheet referencing that attribute updates accordingly.

 

Regards, Ben

Re: Tabular note update affecting all sheets in draft

Experimenter
Experimenter

Yes it is a single part file with several sheets. Can i perform that attribute creation for a full tabular note?

Re: Tabular note update affecting all sheets in draft

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @SergioG,

 

Does this help?

 

(view in My Videos)

 

Regards, Ben

Re: Tabular note update affecting all sheets in draft

Experimenter
Experimenter

Yes, thanks!