Cancel
Showing results for 
Search instead for 
Did you mean: 

Tag drawing title block scale to: N/A ?

Genius
Genius

Hello

Why must I put a scale to a drawing like 1/2, 1/5 why can't I just write N/A because I have lots of different scales at the same time on a drawing ?

  • I never use the real scale(mentioned on title block) on all base views so I want the title block to say SCALE: N/A. So no one makes the mistake believing the drawing is as the scale says.
  • The Scale seems to be always visible on the company template so I can't remove it. Just make it say N/A.
2 REPLIES 2

Re: Tag drawing title block scale to: N/A ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

They are probably using the drawing sheet attributes to set the text for the scale (see docs here:

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:drawing_drw_auto_text_ov)

 

I don't know a good way of over-riding it.

Do your drafting standards allow "X"ing out the "box" where this data is shown?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Tag drawing title block scale to: N/A ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Filed IR 7905996 to allow this.

I'm assuming it will be turned into an ER.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled