Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Attribute - Alternate ID

Pioneer
Pioneer

Hi All

 

Does anyone know how to map the TC attribute "Alternate ID" in Drawing file.

 

"Alternate ID" is ID assigned by a company to their part in Teamcenter ID.

EX: Say TC id is DB0123456, which will be assigned with alternate ID 10020325.

I tried in Annotation->Relationship->Import Part Attrribute. It is showing the attribute in it.

 

Thanks in Advance

Sathyaraj C

NX9.0 | TC 10

2 REPLIES 2

Re: Teamcenter Attribute - Alternate ID

Creator
Creator

Anyone figured this out?

Re: Teamcenter Attribute - Alternate ID

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Akshay380 

 

The last few cases that we [GTAC] had were converted to ER (ER 6608206) and are currently still open.  At the time, attribute mapping was attempted and using occurrence notes, but both failed.

 

I did find the following, which I have not tested:

 

Alternate IDs are runtime properties on the Item/ItemRevision. These do not map to NX. This is also an issue because there can be multiple alternate IDs on an ItemRevision.  Several Enhancement Requests (ER) have been submitted requesting this ability.  As a workaround, if only one alternate id is used, the value can be mapped ONLY if the Teamcenter Display Rule is set to display the alternate ID as the ItemID, rather than the Teamcenter ItemID.


The mapping would be as follows:
{ Dataset type="UGMASTER"
    # (hard-wired) DB_PART_NAME : "Part Name"
    # (hard-wired) DB_PART_DESC : "Part Description"
ALT_ITEM_ID : Item.current_id /master=iman /description="Part Number"
ALT_REV_ID : ItemRevision.current_revision_id /master=iman /description="Part Revision"
}
{ Dataset type="UGPART"
    # (hard-wired) DB_DATASET_REV : "Part File Rev"
    # (hard-wired) DB_DATASET_ID : "Part File ID"

ALT_ITEM_ID : Item.current_id /master=iman /description="Part Number"
ALT_REV_ID : ItemRevision.current_revision_id /master=iman /description="Part Revision"
}

 

Please consider contacting GTAC to ask that you're added to the ER.

 

Regards, Ben