Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter uses a different NX9 ?

Genius
Genius

Hello (My company started using Teamcenter)

Why Teamcenter uses a different NX9 that does not use my own Customer Defaults that I inserted earlier into my original NX9 that was there before Teamcenter arrived ?

 

  • How do I change the Customer Defaults in the Teamcenter's NX9 ?
  • Teamcenter-> Start/Open in NX-> launches a different NX9 that does not have my Customer Defaults ?
3 REPLIES 3

Re: Teamcenter uses a different NX9 ?

Honored Contributor
Honored Contributor

That is dependant on how your company has things setup.  We store our customer defaults on a server, so I can move any native settings to the teamcenter area, and visa-versa.  I'd talk to you Tc/NX admin, and see what they can do to help you.

 

I'd also encourage you to save a "role" once you have things how you like, then you can quickly bring things back, if something again changes (new computer, etc)

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Teamcenter uses a different NX9 ?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can export the customer defaults settings from native NX and import to TC-NX using Defaults Level as 'User'

 

customer_defaults1.PNG

 

 

customer_defaults.PNG

 

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Teamcenter uses a different NX9 ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note that TC starts NX via a .BAT somewhere in the *TC* install folder, e.g. in TC2007, it is ...\rac\start_nxmanager.bat

In TC11, it is ...\portal\start_nxmanager.bat

 

What I would suggest is that you open an "native" NX session, list the log file (File -> Help -> Log file) then save the "info" window to a text file.

Then open an NX session from TC, and save the log file to a different text file.

Compare the 2 text files to make sure that the ENV variables are the same (except for differences required by TC).

 

Especially UGII_SITE_DIR, UGII_GROUP_DIR, and UGII_USER_DIR (but others may apply).

If you start native NX using a .BAT that sets a bunch of ENV variables to values different that the "out of the box" install, you will have to replicate setting those ENVs in start_nxmanager.bat

 

Hope this helps...Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled