Cancel
Showing results for 
Search instead for 
Did you mean: 

The problem with Rapid Dimension

Creator
Creator

I meet that warning: "jog end offset must be less than the start offset"

 

resuilt.PNG

 

 

when using Rapid Dimension in Sketch, PMI and Drafting. How do I solve it?

 

PMI.PNGdrafting.PNGmodel.PNG

2 REPLIES

Re: The problem with Rapid Dimension

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The warning show what is wrong.

If you go to your drafting setting, (is also working for sketch and pmi dimensions)the end offset of the jog can be bigger then the start offset.jog error.JPG


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: The problem with Rapid Dimension

Creator
Creator

I still set that's no jog as default. But, when I turn jog style, it show:
Capture.PNG

 

I have just changed End Offset parameter to 2. But, it return to 5 when I create a new model. So, how can I set it default?