Cancel
Showing results for 
Search instead for 
Did you mean: 

Thread is not marked along the entire length in draft

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

I  made tread hole and then I made intersection.  When I go to draft to make section view the thread is not marked along the entire length (check photo nr 2)

 

model.png

 

2.png

 

What could be reason?  Are you able to help me?

 

14 REPLIES 14

Re: Thread is not marked along the entire length in draft

Siemens Legend Siemens Legend
Siemens Legend

Hi @lukipap ,

Please change depth type to 'Full' from thread dimensions. It might help.

Thanks,

Amol

Re: Thread is not marked along the entire length in draft

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi, thanks for respond but I set already "full" and it doesn't help me Smiley Sad

 

3.png

 

Do you have any other idea?

 

Best regards

Lukasz 

 

 

Re: Thread is not marked along the entire length in draft

Phenom
Phenom

Does it work if you take the interruption out of your part?  

Re: Thread is not marked along the entire length in draft

Siemens Phenom Siemens Phenom
Siemens Phenom

@lukipap , I'm afraid, you can't do that as hole is broken in 2 portions. However, you can display it by adding sketch lines in other portion.

You can cosider opening an ER with GTAC .

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Thread is not marked along the entire length in draft

Honored Contributor
Honored Contributor

What if you put the slot in after the threaded hole?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Thread is not marked along the entire length in draft

Phenom
Phenom

Hi @SamadhanGaikwad ,

there is an ER opened for this situation. Sure @BenBroad can share here the ER in the manner that @lukipap can add itself to the ER.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Thread is not marked along the entire length in draft

Siemens Phenom Siemens Phenom
Siemens Phenom

@cubalibre00 , @lukipap , Below is the internal ER which requests the same:

 

ER7256282: The thread silhouettes are shown partially along length of the threaded hole.

 

ThreadSilhouettesPartiallyDisplayed.JPGThread silhouettes partially displayed

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Thread is not marked along the entire length in draft

Siemens Phenom Siemens Phenom
Siemens Phenom

In this case, it is designed behaviour. For threaded hole, cylindrical face is splitting into two disconnected faces and thread will be positioned on the face which will near to the thread origin.

 

Couple of workarounds that can be used:

1) Create general hole and apply separate threads to cylindrical faces

 

2) Split into two bodies

     Create threaded hole with Boolean operation as none

     Subtract hole body from one of the split body (Keep tool body)

     Subtract hole body from other split body

     Unite split bodies

Re: Thread is not marked along the entire length in draft

Siemens Phenom Siemens Phenom
Siemens Phenom

The 'Thread' feature is applied only to the FACE of the Hole, not to the Hole feature itself.  This means that when the face of the Hole was 'split' into two faces, only one of the faces retained the original object tag and therefore that's the one the Thread feature remains applied to.  The other half of the Hole feature, its face has a new object tag and thus has no Thread feature assigned to it.  If all you want is to make the view in the Drawing look correct, simply apply a second Thread feature to the face of the other half of the Hole.  However, I agree that it would better if the Thread feature were enhanced such that it's applied to the face(s) of the Hole feature, no matter how many faces that might be, in this case two faces.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA