Cancel
Showing results for 
Search instead for 
Did you mean: 

Thread type in NX10 hole command

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Where did the thread type go in the hole command in NX10? In 8.5 I was able to change the thread type to fine, course, helicoil, etc. Is there a setting I need to change?

Thanks

Joseph

2 REPLIES

Re: Thread type in NX10 hole command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Expand the "settings" section of the dialog, pick the thread type from the "standard" drop down box.

 

If you don't see the "settings" section of the dialog, press the little gear icon in the upper left corner of the hole dialog and choose "Hole (more)".

Re: Thread type in NX10 hole command

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Thank you very much!