Cancel
Showing results for 
Search instead for 
Did you mean: 

Thread using No of turns

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello all,

I've tried to create a thread on a cylinder where in which we have 2 options either symbolic or detail..in symbolic we have an option called No of turns we need...so in the same way in detailed thread method is there a way to create a thread using that option or is there any other method to create a thread.???
2 REPLIES

Re: Thread using No of turns

Siemens Phenom Siemens Phenom
Siemens Phenom

I would use a pair of Suppress-by-Expression entries to suppress one Thread feature while unsuppressing the other.  If you use a common expression value to do the switch then you only have to edit a single value to get the result that you want.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Thread using No of turns

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks @JohnRBaker Smiley Happy