Cancel
Showing results for 
Search instead for 
Did you mean: 

Through Curve mesh Continuity

Creator
Creator

Hello, I started to use NX recently, and I have a doubt about Through curve mesh continuity. 

I was designing a bottle and I used "Through Curve mesh" to create the body. When I make G1(tangent) in the continuity group, with another face of the bottle the model volume differs when there is no G1 continuity constrained.

My problem is that, does G1 (Tangent) continuity constraing has a effect on model volume of the design?

I hope I made myself clear to you guys, if not please tell. 

4 REPLIES 4

Re: Through Curve mesh Continuity

Legend
Legend

Hi @BHANU_1

 

The G1 continuity always lead to changing shape of its resultant surface.

So you cannot avoid changing of the volume.

 

But, if you want, you can use (Axi-symmetric) Scale the result body to change the volume, additionally.  

 

ps) As i think, you can use Optimization Tool to get the desired scale factor.

 Sunkap Ahn, Senior Support Engineer


logo

Re: Through Curve mesh Continuity

Creator
Creator

Thanks Skahn. I want to know is it necessary to put "continuity" when using Through Curve Mesh? and can you please be more specific about previous answer

Re: Through Curve mesh Continuity

Legend
Legend

@BHANU_1 wrote:

Thanks Skahn. I want to know is it necessary to put "continuity" when using Through Curve Mesh? and can you please be more specific about previous answer


 

If you not put G1 'continuity', the results will create 'sharp edges' between its adjacent faces.

 

As you knew, you can remove the sharp edge with Edge blend.

But the un-intentional (partial) sharp edges can make problem to  edge blend.

 

 Sunkap Ahn, Senior Support Engineer


logo

Re: Through Curve mesh Continuity

Legend
Legend

If you want information about 'Optimization to get Scale factor for specify volume.'

 

 

 

Please try as below

 

1. Create Volume Expression by Measure body with Associative. [Vol0]

2. Use Axi-symetric Scale for the body and modify name expression. [Along1=1, Other1=1.05]

3. Create Volume Expression. [Vol1] (it is target volume, be careful about uint mm^3 )

4. Create user Expression as constant (not length or area). [Error=(Vol0-Vol1)^2]

5. Use Optimazation [Analysis > Optimazation and Senstivity > Optimazation]

    - Objective : Type=Minimum, Expression=Error (of Step4)

    - Variable Expression :  Other1 (of Step2) [lower and upper limite=0.9 & 1.1]

 

Optimization tool may keep to change Other1 until Vol1 = Vol0.

 Sunkap Ahn, Senior Support Engineer


logo