Cancel
Showing results for 
Search instead for 
Did you mean: 

Thumbnail of files in History

Legend
Legend

Hi

 

I curious about the behaviour in our NX.

Sometimes I can see thumbnails of the files that have been open in NX when I go to the "History" tab.

But the next day I can open NX and then it's just showing the NX icon. And sometimes it's showing some thumbnails of some files but not all.

We are running NX together with Teamcenter and it's in managed mode.

 

It's not a big disaster but still a bit annoying so if somebody can explain why NX behaves like this and what can be done when it occurs.

 

Jörgen

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018
1 REPLY 1

Re: Thumbnail of files in History

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

I have encountered it sometimes with parts in an assembly so we generally set PART PREVIEW creation time setting to ON SAVE and generally open the assembly and do a FORCE SAVE ALL for generating previews of any leftover part. I am sure there should be a journal/programming tool to do the same.

Best Regards

Kapil