Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Tif image not showing in drawing

Creator
Creator
Hello,

I am trying to create a NX drawing containing a tif image. What I first did was creating a model containing an extruded body. Then, I used the raster image option to place a tif image on one of the faces of the body. However, when I used the model in a drawing, I only see the body without the image. Is there a way to resolve this issue?
2 REPLIES 2

Re: Tif image not showing in drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you are using the master model drawing method (part is a component of the drawing file), make sure the image is included in the model reference set; or create a new reference set for use in the drawing. By default, NX only adds solid and sheet bodies to the model reference set.

Re: Tif image not showing in drawing

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
If you're not using master model drawing method (part is a component of the drawing file), make sure the layer on which you placed the rastor image is visible in the views on the drawing.