Cancel
Showing results for 
Search instead for 
Did you mean: 

Title Block: Display Filename of Referenced Part

Creator
Creator

I'm modifying the sample Title Block to use as our standard. The filename of the part I've got in the Drawing is "NX11 SAMPLE PART," so naturally the Drawing Number displayed in the Title Block is the default filename of the Drawing, "NX11 SAMPLE PART_dwg1."

 

In our system (not using Teamcenter integration) the Filename of the Part is the Drawing Number, so I'd like to have the the Filename of the referenced part - not the filename of the drawing - displayed in this cell of the Title Block.

 

Can anyone tell me how to access that data for display?

2 REPLIES 2

Re: Title Block: Display Filename of Referenced Part

Honored Contributor
Honored Contributor

I think you will have to use an "attribute template", to port it thru to the drawing file.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Title Block: Display Filename of Referenced Part

Siemens Phenom Siemens Phenom
Siemens Phenom

I think one of these attributes might be what you need. Just replace the existing value in the title block cell with the attribute you need:

 

<W@$SH_MASTER_PART_NAME>
   Master Model drawing sheet part name
<W@$SH_PART_NAME>

   Sheet part name

 

By the way, there are a whole list of system attributes for drawings listed at the bottom of this page:
https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help#uid:index_drafting:id700849:id1268622:id1...