Cancel
Showing results for 
Search instead for 
Did you mean: 

Title Block

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi, I need to have a title block with two parts: main title block positioned  bottom right plus a note up right (see image below). I have done a single title block composing the tabular notes according to my need, and it is ok.

But if I edit the size of the sheet (eg from A2 to A3) I have to manually edit the upper part of the Title Block.

I know it is an obvious behaviour, being a block it behaves like a block, but has anybody a hint to avoid this? I tried making two separate title blocks, but it doesn't work.

Thankyou

title block 01.jpgtitle block 02.jpg

3 REPLIES

Re: Title Block

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I am creating as a separate titleblock objects in different corners of the drawing, & when resizing the drawing sheet, everything moves correctly for me (NX10.0.3.5 MP5 & MP16)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Title Block

Phenom
Phenom

Hi,

the problem is because the upper title block hasn't set the origin associative to.

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Title Block

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Thank you, it works. The first time I tried I forgot to assign Material and
evaluate the weight, that's why I got the error message.