Cancel
Showing results for 
Search instead for 
Did you mean: 

Title box name in NX managed

Genius
Genius

I have the name of the tile box with this callout <W@$SH_PART_NAME>. It shows PART VISUALIZATION NAME+(DWG FILE NAME).

By PART VISUALIZATION NAME I mean the text I see for the revision in NX and in TC which is a chain composed by  ID+REVISION+VERSION+NAME

By DWG FILE NAME I mean the name TC gives to the dwg file (Specification: ID-REVISION-dwg1).

 

I would like to avoid DWG FILE NAME to be shown in this field. I can do it by change the <W@$SH_PART_NAME> callout for callouts for ID, REV and NAME but I would like to automaticaly call the PART VISUALIZATION NAME just in case it is changed in future. Is there a way to call it without calling the DWG FILE NAME)?

 

3 REPLIES

Re: Title box name in NX managed

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
If you have the model part and drawing file in 1 prt file then you can use the <W@$SH_PART_NAME>

if you have the model and drawing part in 2 files (model1 and model1_dwg) then you can use the <W@$SH_MASTER_PART_NAME> This will direct look into the model1 name and skip the drawing name.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Title box name in NX managed

Genius
Genius

Thank you Ruud, <W@$SH_MASTER_PART_NAME>  worked perfectly. 

Is there a list with all available expressions for calling atributtes?

Re: Title box name in NX managed

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

the link below is from the documentation of NX that shows all the default System attributes for drafting

https://docs.plm.automation.siemens.com/tdoc/nx/11.0.1/nx_help/#uid:drawing_drw_auto_text_ov

This is the default list.


 

<W@$SH_SHEET_NUMBER>  =  Sheet number of the current sheet
 

<W@$SH_NUMBER_OF_SHEETS> =  Number of sheets in the current part
 

<W@$SH_SHEET_REVISION>  = Revision letter of the current sheet
 

<W@$SH_SHEET_SCALE_NUMERATOR>  = Numerator of the sheet scale
 

<W@$SH_SHEET_SCALE_DENOMINATOR>  = Denominator of the sheet scale
 

<W@$SH_SHEET_SIZE>  = Size of the current sheet
 

<W@$SH_SHEET_UNITS>  = Units of the current sheet
 

<W@$SH_SHEET_PROJECTION_ANGLE>  = Projection angle symbol of the current sheet
 

<W@$SH_MASTER_PART_NAME>  = Part name of the master model displayed in the drawing sheet.
 

<W@$SH_PART_NAME>  = Sheet part name
 

<W@$SH_SHEET_ZONE> = Sheet zone
 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions