Cancel
Showing results for 
Search instead for 
Did you mean: 

Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

 

Can I know the Topics of NX Cool Shape Design Bundle(NX12300). I mean like does it have Modeling, Drafting, Freeform Basic and Advanced, Freeform Shape, etc.

 

Regards

Raju

8 REPLIES 8

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Siemens Legend Siemens Legend
Siemens Legend

Raju,

 

The NX Cool Shape Design Bundle includes advanced capabilities for developing initial product design assemblies.

It provides surface creation, manipulation, and analysis capabilities including subdivision modeling, class-a surfacing and reverse engineering to enable customers to create aesthetically appealing, innovative products.

It provides users with enhanced visualization with both dynamic and real-time photo-realistic rendering tools.

 

If you need further information, please contact your local Siemens PLM Sales Representative or local siemens PLM Channel Manager.

 

Jerry

- - - -
Jerry Sarfati
Siemens PLM Software

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Dear Sir,

Even I wanted to know the content of cool shape design bundle. In the price book also not much is mentioned. like whether it contains Sheet metal or PMI.

Thanks & Regards
Nadeem Ansari
Om Engineers / CAD CAM Galaxy
www.cadcamgalaxy.com

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

If I am not mistaken, (I am not sure if these are the same for all since Sales people are the one who do this kind of thing).

This are the contents of NX 13200.

-Teamcenter - NX Manager 
-Teamcenter - CAD Manager Server 
-Teamcenter 
-Visualization Base 
-XpresReview 
-Solid & Feature Modeling 
-Assembly Modeling 
-Design Logic 
-Grip Runtime 
-Knowledge Fusion Runtime 
-Process Studio runtime license 
-Translators (IGES, DXF/DWG, STEP 203/214, 2D Exchange) 
-Rapid Prototyping 
-Freeform modeling, basic 
-Straight Brake Sheet Metal 
-Drafting  
-Web Express 
-Process Solutions for Stress and Vibration 
-Check-Mate Runtime 
-User Defined Features 
-3D Annotation (GD&T and PMI) 
-Freeform Modeling, Advanced 
-Molded Part Validation 
-Mold Wizard 

 

Regards,

Sen Cutay

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Sen, what you've posted is the NX13200 Mold Wizard bundle.

 

NX12300 is the Cool Shape Design Bundle.

It contains the following features in the license:

 

assemblies
dotnet_runtime
dxf_to_ug
dxfdwg
features_modeling
gateway
iges
nx_freeform_1
nx_freeform_2
nx_integration
nx_subdivision
pv_ugdatagenerator
sla_3d_systems
solid_modeling
step_ap203
step_ap214
studio_analyze
studio_free_form
studio_render
studio_visualize
teamcenter_designer
ug_to_dxf
ugopen_menuscript
visview_base

 

It has all the modeling functionality (solid, freeform basic and advanced, realize shape).

It also has the rendering and analysis for advanced freeform.

 

It does not have drafting,  sheetmetal or PMI.

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hi Anthony,

I see. ( I told you I wasn't sure Smiley Very Happy)

Regards,
Sen

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks, That solves my requirement Smiley Happy

Thanks & Regards
Nadeem Ansari
Om Engineers / CAD CAM Galaxy
www.cadcamgalaxy.com

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Siemens Legend Siemens Legend
Siemens Legend

For anybody not well versed in licence bit speak.

 

NX Cool Shape Design contains all the Solid, Surface & Assembly tools along with NX Realize Shape.  So it's focus is on model creation and visualization

 

It does not include Drafting, PMI or UDF functionality.

 

Paul

Re: Topics of NX Cool Shape Design Bundle(NX12300).

Experimenter
Experimenter

Hi.

whats the difference between "NX Cool Shape Design" and "NX Shape Design" addon?

Thanks