Cancel
Showing results for 
Search instead for 
Did you mean: 

Transfering from nx10 to nx11

Valued Contributor
Valued Contributor

Hi,

I was wondering if there was a good way to transfer my customer defaults from nx10 to 11. I also have custom templates that I use for modelling and some for drafting that I need to bring over also. I was wondering if there was a way to do this without copy / pasting all the files into the new nx11 folders. Something that is more reliable and efficient.

Thanks

 

1 REPLY

Re: Transfering from nx10 to nx11

Siemens Phenom Siemens Phenom
Siemens Phenom

The best thing to do for customer defaults is to go into NX 10, Manage Settings and then export them. From there go back in NX 11 and do in import to get the customer defaults to come over. 

 

As for the seed files for design and drafting, they need to be either copied to a new location of update the NX 11 .pax files to use the ones you have. 

 

The image below shows the menus for exporting and importing the customer defaults. This is the best way to move them forward from version to version on NX.

 

Scott

 

ManageDefaults.png