Cancel
Showing results for 
Search instead for 
Did you mean: 

Trim linear or circular pattern

Creator
Creator

Hello to everyone,

 

Is it posible to trim lines of pattern, from outside or inside of parallelogram, but not to lose reference for pattern.

 

Trim.JPG

Thank you!

 

I use NX11.

 

2 REPLIES

Re: Trim linear or circular pattern

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

There are several things you could do here.

Let me inspire you with two of them.

 

1. Pattern the sketch feature

If you trim a single curve of the second sketch to the boundary of the first sketch (rectangle) then you can create the pattern as a feature pattern. In pattern feature you pattern the sketch with the single curve, while in the reuable references group you select the external refernece form the first sketch. 

 

2. Project all the patterned curves to a sheet

If you want to contain the inner portion then you can create a sheetbody (extrude the rectangle over 0mm to get a sheet) and then project the curve pattern (the second sketch) to the sheet. The result will give you all the curves that are within the sheet boundary.

 

Have fun!

 

Regards, **bleep**

 

01 sketch.PNG01 pattern sketch.PNG03 pattern result.PNG

 

 

 

Re: Trim linear or circular pattern

Creator
Creator

Hello DickBaardse ,

 

Thank you very much. Second solution is better for me.

 

Best Regards