09-20-2016 11:03 AM - edited 09-20-2016 11:23 AM
See attached photo. I am trying to model this, but the radius on the tensile specimen is kind of "stretched out". Simply using the fillet tool (with a .250 radius fillet) doesn't work. What do I need to do to make the radius?
This is a FLAT specimen not a cylindrical specimen!
Thanks
Solved! Go to Solution.
09-20-2016 11:19 AM
09-20-2016 11:21 AM
09-20-2016 11:22 AM
09-20-2016 11:23 AM - edited 09-20-2016 11:32 AM
Yeah, I just saw that. Sketch the profile and extrude it.
Edge Blend should also work (this was with default settings and just dragging handles):
Ben
09-20-2016 11:23 AM
09-20-2016 11:30 AM
"Simply using the fillet tool (with a .250 radius fillet) doesn't work."
Do you get a message about "not able to terminate blend face..."?
If so, in the edge blend dialog, expand the "overflow resolutions" section and turn on the "allowed overflow resolution" options (all three). Turning these options on will allow what used to be known as a "cliff edge" blend.