Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Trouble with importing file

Pioneer
Pioneer

Hi everyone,

I have a small problem with adding the suffix from the imported source file. When I import STEP file "body.stp", the name of file was change to "body_stp.prt". What can I do to import file without the suffix from source file in the name?

 

Jack1

4 REPLIES 4

Re: Trouble with importing file

Phenom
Phenom

Hi @Jack1,

it's not possible.

Thank you...

Using NX1867
RuleDesigner PDM

Re: Trouble with importing file

Gears Phenom Gears Phenom
Gears Phenom

Use the Translator Tool GUI outside of NX.

gui.jpg

Re: Trouble with importing file

Gears Phenom Gears Phenom
Gears Phenom
You can work around this issue in 2 ways:

1. Use the external translator as already mentioned.

2. Use File -> New -> Blank template or Open an existing start part and then use File -> Import -> STEP203 or STEP214.

The issue is that you're trying to open the STEP file rather than import it. This affects the name of the resulting NX file.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6

Re: Trouble with importing file

Pioneer
Pioneer
Thank you! Both solution are working Smiley Very Happy