Cancel
Showing results for 
Search instead for 
Did you mean: 

UI: NX Theme, which one do you prefer

Creator
Creator

Hello,

 

I'm working with NX 19 Years ago. Since Unigraphics V15.
So I've seen some different UI's in all the time. Some things are now better, some not.

 

 

Which of the NX Thems for the UI do you prefer?

The pictures her are captured from NX1847.

 

NX_UI_Themes.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Since the "Light (Recommended)" is appeared much people work with them.

But I'm not satisfied with that. It has too little contrast, and anityhng is in white to light gray.
And with the Windows 10 (2 Dimensional?!?) design, it's much difficult to see where a window begins and ends.
 
NX_UI_Theme_Light.png
 
 
The "Light Gray" is'nt really an alternative for me. Looks as the same, but gray in gray.
 
NX_UI_Theme_Light-Gray.png
 
 
My Favorite: "Classic with System Fonts"
It gives good contrasts, particular in CAM menues.I see much more better where windofs begins and ends.
Why "with System Fonts? Well, the characters are a bit narrow, so there I can se more of them in the input fields.
Yes, I like it.
 
NX_UI_Theme_Classic-with-System-Font.png
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
An then the "System" theme. It looks not bad, but I don't like it. There are no lines in the ONT.
The only interresting thing is the red or blue arrows for collapsed/uncollapsed parts of menues.
 
NX_UI_Theme_System.png
 
 
Why am I talking here about that?
I'm afraid, in future the different themes will desappear. Then ther is only one unit theme and maybe
it's not my preferred theme.
 
What is your opinion?
 
 
 
Regards
TomS
 
 
 
10 REPLIES 10

Re: UI: NX Theme, which one do you prefer

Honored Contributor
Honored Contributor

Until a couple weeks ago, I never changed the theme, and only then because of the discussion on the NX1847 icon colors.  Since UG v8, I've just used whatever the default was.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: UI: NX Theme, which one do you prefer

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

# TBT (Throw-back-Thursday).  Bonus points - guess the version:

 

Screenshot - 3_14_2019 , 11_23_49 AM 002.png

 

Regards, Ben

Re: UI: NX Theme, which one do you prefer

Valued Contributor
Valued Contributor

Since about NX 5 (pretty sure that was the version I started on) I have used the Light - recommended theme.

 

Re: UI: NX Theme, which one do you prefer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@BenBroad, I'm guessing UG v16.

Re: UI: NX Theme, which one do you prefer

Gears Phenom Gears Phenom
Gears Phenom

@BenBroad wrote:

# TBT (Throw-back-Thursday).  Bonus points - guess the version:


UG v15?

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: UI: NX Theme, which one do you prefer

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

@cowski1 wrote:

@BenBroad, I'm guessing UG v16.


Oh man... that was way too easy.  Congratulations Cowski - your prize is a kudos!

Re: UI: NX Theme, which one do you prefer

Honored Contributor
Honored Contributor

@BenBroad wrote:

# TBT (Throw-back-Thursday).  Bonus points - guess the version:

 

 

Regards, Ben


"orphans", wow, I don'te even remember that one.  ...maybe UG v12? 

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: UI: NX Theme, which one do you prefer

Gears Phenom Gears Phenom
Gears Phenom
@BenBroad,

Back then grayscale icons meant not selectable. Look how far we've come (sarcasm). Heh heh.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: UI: NX Theme, which one do you prefer

Siemens Legend Siemens Legend
Siemens Legend
TomS,
I agree with you. I do not like the Windows10 -2D appearance.
Every n-th year a new batch of engineers/designers/programmers/whatever takes the scene and says :
"Look at this ! this new scheme is way revolutionary!"
and for some unknown reason we let these guys have their way when really we should build on what we have learnt before.

Regards,
Tomas