Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to delete Array master

Master
Master

I had put a components in an assembly as arrays. I am trying to delete all instances and it won't let me delete them with the following error. Any ideas? Thanks

 

The following component could not be deleted

"part number" Attempt to delete and array master component failed.

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
8 REPLIES 8

Re: Unable to delete Array master

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

delete the array first

 

2017-01-12_10-54-12.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Unable to delete Array master

Master
Master

I figured I was missing something. Would not have looked for it there for sure! I figured it would have been in the right click menu. Thank you sir!

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Unable to delete Array master

Master
Master

We just updated to NX 11. Where did this command go?

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Unable to delete Array master

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

From the Assembly Navigator, you can delete the master array from the Component Patterns node by right clicking the pattern (LinearPattern, CircularPattern) and choosing Delete.

Regards, Ben

Re: Unable to delete Array master

Master
Master

Thank you sir! Appreciate the help!

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Unable to delete Array master

Experimenter
Experimenter

In my assembly, the "Delete Array" button on the "Display Component Arrays" dialog is greyed out.
Are there any other ways to delete the array and component?

 

Clarification: I am using NX8.5

Re: Unable to delete Array master

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @mikescurfield,

 

I assume you're using a version of NX earlier that NX 9.  I've tried various ways to get the Delete Array option to be greyed out (component suppression, unloaded masters, nested arrays, to mention a few), but I can't reproduce the issue, nor do we have any records suggesting that anyone has reported this to GTAC in the past.  In one case Edit Parameters was greyed out, but that was because an instance array was controlling the component array.  It almost seems like there might be some higher level influence that's controlling your array.

 

Did you try "File > Utilities > Part Cleanup" with all Moderate Cleanup Actions checked?

 

If you can't upload your parts here (in a zip file), may I suggest that you open an IR with GTAC and have them review the part?

 

Regards, Ben

Re: Unable to delete Array master

Experimenter
Experimenter

@BenBroad, Thanks for the suggestion. Part Cleanup did not resolve the issue, so I will probably end up replacing the entire installation model