Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to map unit definition g/cm^3 for parameter MassDensity

Legend
Legend

I try to assign Material from Classification library where in MatML dataset defined units for Density in
g/cm^3

 And as result I've got that error - Unable to map unit definition g/cm^3 for parameter MassPropsDensity.

 I also found that units in kg/m^3 works fine, but if I change units to g/cm^3 - this error occure.

I saw one PR on GTAC site with similar problem -PR #:7732439

 Unable to map unit definition mm^2/N(1/MPa) for parameter Volumetric Deformation Constants

 But there is no workaround for that PR, only recommendation to try this in NX11

 
Does workaround for this subject exist?



1 REPLY 1

Re: Unable to map unit definition g/cm^3 for parameter MassDensity

Legend
Legend

It was a localization issue. Closed