Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to rotate part (only SIM file)

Pioneer
Pioneer

 

 Hi all.

 

Not sure where this post belongs, but I just got a problem with rotating the part in the SIM file. All other files works fine and even if I load the results in SIM file I can rotate the part. But not when I am in the main window in SIM file.

 

Trying to figure out if I have "locked" the rotations somehow but cannot figure it out.

 

Picture below shows that the rotation button is dark/grey and I an unable to click this button. I do use a 3D mouse, but the 3D mouse (and regular mouse) works fine in all other files as mentioned.

 

Also when I click right mouse button the rotation field is missing!!

 

I can do following things:

 

- Pan all direction with mouse

- Zoom in/out with middle mouse button

-  Use fit button

 

I cannot do:

- rotate with mouse

- use the view / orient buttons to change the orientation of the part

- Click the rotation button

 

Any ideas anyone??

 

Thomas

 

 

 

Unable to rotate.jpg

 

 

 

1 REPLY 1

Re: Unable to rotate part (only SIM file)

Experimenter
Experimenter

Hi,

I had the same problem in NX11 but only when plotting FEM results. I am using a SpaceMousePro and for some reason it seems like the "lock/Unlock Plane" function have some hickups. I turned it on and then off and then it worked fine.

 

Hopes this helps for you as well.

 

Best regard

 

1.png