Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to some functions in Managed NX

Experimenter
Experimenter

Windows 7 X64
Teamcenter 10.1.4.2(64Bit)
NX 8.5.3.3(64Bit)

 

I found some difference between managed mode & native mode.

 

IN MANAGED MODE, 'Composite Curve', 'Extract Body' and 'Mirror Body' are appeared on Associative Copy Menu.

 

IN NATIVE MODE, they are not available but added some new functions such as' Pattern Feature' and 'Isolated Object of Feature'.

 

And I know that 'Pattern Feature' function is available in Modeling Application but the 'Command Finder' said "it is available in Ship Design Mode" and can't run it.

 

I'd like to use functions appeared in native mode.

 

Please see below pictures.

 

I would be appreciated if you could help me rectify this problem.

 

 

 

* Managed mode:

cam1.jpg

CF1.JPG

 

 

 

* Native mode:

cam2.jpg

 

CF2.JPG

 

1 REPLY

Re: Unable to some functions in Managed NX

Siemens Phenom Siemens Phenom
Siemens Phenom

THIS IS NOT CONTACTING GTAC!!!!!!!

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA