Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Units in Material Library

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

The Help doc mentions two environment variables UGII_UNITS_WRITE_FILE, and UGII_UNITS_DEFINED_FILE, so I think I must either edit the env file, which I can not, or set them as system variable, which I can not. Am I wrong?

Re: Units in Material Library

Gears Phenom Gears Phenom
Gears Phenom

If you start NX using a BAT file you can set whatever environment variables you like in there. These will override whatever NX finds in it's ENV files.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Units in Material Library

Gears Phenom Gears Phenom
Gears Phenom

@Laurus,

You might be able to set the environment variable from the Windows user level versus system level. In Win7, it's Control Panel -> User Accounts -> Change my environment variables. There should be two different areas where environment variables can be entered with the uppermost area being the user environment variables which will only affect your account and no others.

 

But if you're using templates or start parts, by all means go that route if you feel it's easier.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6
Highlighted

Re: Units in Material Library

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

ok, thanks a lot to everybody.  I will try and decide wether to edit the template or to set the variables in the bat file