Cancel
Showing results for 
Search instead for 
Did you mean: 

Updating Customer Defaults in seed file

Gears Phenom Gears Phenom
Gears Phenom

NX 9

 

Is there a quick, way to update all the Customer Defaults in the company seed file?  Sometimes I'll experiment with settings in test files, and later update the master "seed" file.  Just as a sanity check I'd like to make sure all the settings in the seed file are up to what I have set in the Customer Defaults.  Does File, Menu, Drafting Standard update everything, or only the drafting standard settings from the Customer Defaults?  Is there a one stop shopping way to update everything from the Customer Defaults?

 

Thanks,

 Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10