Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Use a part to pattern along contour of another part

Creator
Creator

Hello, everyone, sorry for so frequent seeking answers here.

But I really want to know something a little unique, here is the thing,

I want to make a pattern, and I add two exact the same parts into assembly, and 

what I want to do is to make the part do the pattern "along" the contour of another one.

 

 

Can NX 10 work this out ? Anyone has any ideas about this? 

Thank you so much.

5 REPLIES 5

Re: Use a part to pattern along contour of another part

Phenom
Phenom

Check this out:

https://community.plm.automation.siemens.com/t5/NX-Design-Knowledge-Base/Intelligent-Design-Automati...

 

What kind of part (2X) do you want to pattern?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Use a part to pattern along contour of another part

Creator
Creator

@mike_fdo
Thank you.
But what I want to pattern is part(a model) instead of feature.

OKay, here's the example.  I didn't finish the whole image, but it's pretty much like this,

imagine the Ellipse is a 1-mm sheetmetal, and Arrow is another 1-mm sheetmetal, so they are exactly two different models, AND I want to make Ellipse model pattern along the contour of Arrow model. Hope there's a way for solving this out. THX!

未命名.png

 

 

 

Re: Use a part to pattern along contour of another part

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @knockitover,

 

Have you looked at Create an along path patterned component?

 

Regards, Ben

Re: Use a part to pattern along contour of another part

Phenom
Phenom

Check this out!

 

In the Assembly part; add / delete / modify following sketch's points and also try editing any other sketches as well to check parametric behaviour!

 

 EDIT: ADDED NX10 MODELS "mf_arrow_elps_asm_20180604_NX10"image.png

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Use a part to pattern along contour of another part

Creator
Creator
@mike_fdo @BenBroad Thank you guys so much!