06-01-2018 06:49 AM
Hello, everyone, sorry for so frequent seeking answers here.
But I really want to know something a little unique, here is the thing,
I want to make a pattern, and I add two exact the same parts into assembly, and
what I want to do is to make the part do the pattern "along" the contour of another one.
Can NX 10 work this out ? Anyone has any ideas about this?
Thank you so much.
Solved! Go to Solution.
06-01-2018 08:40 AM
Check this out:
What kind of part (2X) do you want to pattern?
06-04-2018 03:38 AM - edited 06-04-2018 04:07 AM
@mike_fdo
Thank you.
But what I want to pattern is part(a model) instead of feature.
OKay, here's the example. I didn't finish the whole image, but it's pretty much like this,
imagine the Ellipse is a 1-mm sheetmetal, and Arrow is another 1-mm sheetmetal, so they are exactly two different models, AND I want to make Ellipse model pattern along the contour of Arrow model. Hope there's a way for solving this out. THX!
06-04-2018 10:44 AM
06-04-2018 12:18 PM - edited 06-04-2018 06:11 PM
Check this out!
In the Assembly part; add / delete / modify following sketch's points and also try editing any other sketches as well to check parametric behaviour!
EDIT: ADDED NX10 MODELS "mf_arrow_elps_asm_20180604_NX10"
06-05-2018 01:51 AM