Cancel
Showing results for 
Search instead for 
Did you mean: 

User Defined PMI

Experimenter
Experimenter

Hello all,

              I am trying to create a user defined PMI object and insert it my model. I created custom PMI objects by defining them in a DFA file (for test it creates a line). As described in the prerequisite, I set the the knowledge fusion search directories by Preferences→Knowledge Fusion - this pointing to the directory where I saved my DFA file.

When I click on PMI->User defined PMI annotations user_defined.gif  I am getting the following error

Error.JPG

 

Is there anything else am I missing out? 

TIA

 

Shankar J

3 REPLIES

Re: User Defined PMI

Experimenter
Experimenter

You need to set KF search directoty where custom PMI are available

Re: User Defined PMI

Genius
Genius
Can you give some more information how you use "user-defined PMI"? I am not sure what can be done with this features but it seems to be very interesting.

Re: User Defined PMI

Experimenter
Experimenter

I'm having the same issue. I try to set this using: File-->Prefs-->Knowledge Fusion... but I still get the same error.

 

There are no issues with finding my other dfa files in the directory; it is just trying to use the User Defined PMI that gives me this error.

 

I have also followed the "Advanced users Customize NX-supplied DFA-based PMI symbols" help document without effect.

 

Anyone have any success with this?