Cancel
Showing results for 
Search instead for 
Did you mean: 

Using Microsoft Application Virtualization for Deploying NX

Experimenter
Experimenter

Anyone using Microsoft Application Virtualization (AppV) for deploying NX to clients?

 

If you're unfamilar with AppV it basically provides a mechanism to deploy software packages to clients and then run them in a virtual shell on the client (including virtual env vars, virtual registry settings, virtual directories, etc).

 

I'm using AppV to deploy NX11. The package is getting delivered without issue and NX is runniing in the virtual environment, but on some machines NX hangs during basic operations and never returns. The client package has the correct number of NX files/folders. The permissions are correct. The problem occurs irrespective of user. Anyone see this type of behavior?

 

Thanks,

Mike Brown

1 REPLY 1

Re: Using Microsoft Application Virtualization for Deploying NX

Experimenter
Experimenter

Update:

Upgrading to AppV 5.0 SP3 (previously on SP1) resolved the issue. NX11 now consistently works in the Microsoft Application Virtualization environment.