Cancel
Showing results for 
Search instead for 
Did you mean: 

Using journal across multiple components at one time

Experimenter
Experimenter

I am currently in the process of updating an assembly which contains upwards of 2500 components. Part of that update involves modifying the layer categories for each component. As of right now, this is done by making the desired component the displayed part, and running a journal that I created which assigns each category respectively. As one can imagine, this is very time consuming and extremely inefficient. 

 

Is there a way that I can approach this where I don't have to touch each component individually, instead running one command that modifies all of the components in one shot? 

 

Thanks in advance

 

NX 9.0.3.4 MP15

1 REPLY 1

Re: Using journal across multiple components at one time

Valued Contributor
Valued Contributor

I hope adding this part to your existing journal will help:

 

http://nxjournaling.com/content/creating-subroutine-process-all-components-assembly