Cancel
Showing results for 
Search instead for 
Did you mean: 

Using user ID atribute from Teamcenter in Nx tabular note

Valued Contributor
Valued Contributor

Hi

I am using my user ID attribute from teamcenter to populate a cell in a tabular note for use in a drawing border template, but the output is lower case. Does anyone know how to format this to upper case?

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12
4 REPLIES 4

Re: Using user ID atribute from Teamcenter in Nx tabular note

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: Using user ID atribute from Teamcenter in Nx tabular note

Valued Contributor
Valued Contributor

Hi

Cant seem to get this to work.

 

below is what I have in the cell that populates the user ID, can you please suggest how this can be modified to make it uppercase.

 

sorry, its probaly me being a bit thick!

 

<WRef1*0@DRAWING_MODIFIER>

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12

Re: Using user ID atribute from Teamcenter in Nx tabular note

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Open the file that references the TC attribute, start the expression editor and filter for "attribute expressions"; if the TC attribute expression is editable, use the "StringUpper" command to convert the input to upper case. If the attribute expression is locked, create a new string expression that references the TC attribute expression and add the "StringUpper" command. Your drawing note can reference this expression instead of the original attribute.

Re: Using user ID atribute from Teamcenter in Nx tabular note

Valued Contributor
Valued Contributor

Thanks for that, worked perfectly.

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12